Typically, grease is a solid or semi-solid lubricant consisting of a base oil with additional additives and a thickening agent. They are often used in industrial environments, engineering, and automotive applications to keep components moving freely and smoothly. Some greases also offer protection to components against corrosion, as well as wear and tear and seizing.
Greases are commonly composed of three primary components, which helps to maintain its semi-solid form:
Whilst greases are primarily used for lubricating components and moving parts to reduce friction, they also help to bolster overall longevity and efficiency of machinery and various other equipment.
Some of these uses include:
When choosing a type of grease, there are several important factors to consider before purchasing. By carefully taking into account these factors, you can be assured that the type of grease you choose will be suited for your requirements.
By carefully evaluating these factors, you can select an grease that best suits your needs.
There are three different types of lubricating greases, boundary, mixed and full film.
The results depend on whether the two greases are compatible or not. If the greases being mixed are not compatible the effect can be less than favourable, with separations and a generally messy situation.
If you need advice about grease compatibility it's best to seek the advice. You can contact our Technical Safety Team here.
NLGI stands for the National Lubricating Grease Institute, who outlined the standard classification for the measure of relative hardness of a grease in a lubricating application. In short, the NLGI is system of rating a greases consistency from 000 (fluid) to 6 (very hard).
Dropping point is the term used to refer to the temperature at which a grease becomes fluid enough to drip.
To ensure you have all the necessary information regarding greases including the guidelines and standards around greases as well as information pertaining to the selection of the right grease, we've gathered a selection of resources, to help you on your journey to selecting the most effective grease product for your needs.