In compliance with health and safety law, employers are required to establish a health surveillance scheme for workers exposed to specific health risks.
Where there is exposure to fluid or mist, it is a legal requirement to carry out health surveillance even when preventative controls, such as fluid quality checks and LEV, are in place.
Control of Substances Hazardous to Health Regulations (COSHH) requires exposure to metalworking fluids by inhalation, ingestion or skin contact to be prevented where reasonably practicable, or failing that, adequately controlled.
Water-mix metalworking fluid deteriorates over time and can become contaminated with harmful bacteria and other contaminants. Monitoring and maintaining fluid quality is key to controlling risk.
To maintain safe and effective fluids, you need to regularly check and correct concentration, pH and bacteria levels.
For more information, see HSE's guidance sheet COSHH MW5: Managing fluid quality (PDF)
The UK Lubricants Association (UKLA), Metalworking Fluid Product Stewardship Group (MWFPSG) and Health and Safety Executive (HSE) have produced a guide with helpful advice for all employers, see Good Practice Guide for Safe Handling and Disposal of Metalworking Fluids
LEV should be fitted to CNC machines where operators are exposed to metalworking fluid mist. It is the key control measure to reduce inhalation exposure to airborne contaminants such as dust, mist, fume, vapour or gas.
Local exhaust ventilation systems are available in a wide variety of sizes, depending on the work area. A typical LEV system will feature:
For more detail see HSE Clearing The Air guide (PDF)
Cutting & coolant fluids are primarily used to lubricate and cool the cutting tools and workpieces during a wide variety of machining processes. They help reduce heat generation, improve surface finish, extend tool life, and enhance machining efficiency. The main goal of these metalworking fluids is to optimise the machining process and maintain tool and workpiece integrity.
When choosing cutting & coolant fluids, there are several important factors to consider that will be dependent on the applications you will be carrying out.
By carefully evaluating all these factors to ensure the cutting & coolant fluid that is compatiable with your application and parts.
Layout fluids also known as layout dye or layout marking fluids, are used for marking and scribing precise lines and patterns on metal surfaces. They are often used in metalworking, welding, and fabrication to guide cutting, drilling, and other machining operations.
Choosing the right layout fluid type for your project is critical. Consider the surface material, visibility, durability, ease of application and removal. The choice of colour can depend on your personal preference or the specific application.
Always follow the manufacturer's recommendations and safety guidelines when working with layout fluids and their associated products
Rust treatments often referred to as rust inhibitors or rust preventatives, are products designed to protect metal surfaces from corrosion and rust formation. They create a protective barrier on the metal surface, preventing moisture and oxygen from coming into contact with the metal and causing rust. They are commonly used in industries where metal parts or components need to be stored for extended periods.
Rust treatments play a crucial role in preventing corrosion and preserving the lifespan of your equipment and parts. When choosing a rust treatments it is important to consider several factors to ensure you select the most effective rust treatment for your application.
All serve a different purpose in preventing or addressing corrosion issues, and the choice of which to use depends on the specific needs and conditions.