Understanding and adhering to the standards and regulations for head protection isn’t just a legal obligation, it’s a critical component of workplace safety and personal well-being. In this busy era of industrial and construction advancements, the significance of wearing the correct headgear cannot be overstated.
Head protection standards and regulations are the result of years of research, real-world incidents and continuous improvement in safety practices. Adherence to these guidelines isn't merely about ticking boxes on a compliance checklist; it's about creating an environment where every individual can perform their duties without the threat of injury. Understanding and following these standards ensures that the head protection used meets established safety criteria, offering real protection against potential hazards.
The UK hard hat regulations referencing the provision, use, and standard of hard hats on construction sites and other locations include:
EN397 specifies the requirements for helmets designed to protect against falling objects and impact injuries, making them a staple on construction sites and other hazardous environments. These helmets are tested for shock absorption, penetration resistance, and flame resistance, ensuring comprehensive safety. Additionally, they may come with optional features like molten metal splash protection and low-temperature performance. If your workplace involves risks of head injuries from falling materials, an EN397-compliant helmet is crucial.
View our range >
Aimed at individuals working at heights or in mountainous terrains, helmets meeting the EN12492 standard are designed for more than just falling objects; they ensure the helmet remains securely on the wearer’s head during a fall. This standard is crucial for climbers, arborists, and anyone involved in height-related work, providing added features such as increased shock absorption and resistance to multiple angles of impact. These helmets typically feature a more secure fit and better head coverage to protect against side impacts, making them ideal for dynamic and high-movement environments.
View our range >
This standard offers a higher level of protection compared to EN397. Helmets certified under EN14052 are designed to provide enhanced protection against high-impact forces and are suitable for industries where workers are at a greater risk from falling or flying objects. They cover more of the head by providing additional protection against side impacts and penetration. If your work environment involves high-risk scenarios, a helmet conforming to EN14052 standards offers superior safety and peace of mind.
View our range >
This standard is specifically for electrically insulating helmets used in low voltage installations. Safety helmets meeting EN50365 standards are ideal for electricians and others working in close proximity to live electrical conductors, equipment, or circuits. They provide protection against electric shocks up to 1000V AC or 1500V DC, ensuring safety during electrical operations. If electrical hazards are a concern in your workplace, choosing a helmet compliant with EN50365 is crucial for preventing head injuries caused by electrical accidents.
View our range >
The Personal Protective Equipment at Work Regulations 1992, is the law that specifies this to be the case. Employers have to manage and plan work accordingly to reduce risks, however if residual risks still remain then PPE must be worn and head protection falls into this category. This will apply to the vast majority of activities.
Ensuring compliance with head protection standards is essential for workplace safety. It is the shared responsibility of employers, employees, and site managers to adhere to safety regulations to prevent head injuries. Here are some simple steps to help ensure you comply:
While the use of hard hats is a critical component of workplace safety on construction sites, there are specific exemptions under UK law. Understanding these exemptions helps maintain legal compliance and respect individual circumstances without compromising overall site safety.
Employers are responsible for providing Personal Protective Equipment, including hard hats, to employees and visitors whenever there is a risk of head injury on the construction site. This is part of ensuring workplace safety and compliance with UK hard hat regulations.
Yes, there are exemptions. One main exemption under UK law is for turban-wearing Sikhs, as specified in Section 6 of the Deregulation Act 2015. Additionally, if a site-specific risk assessment determines no risk of head injury, hard hats may not be required.
Hard hats used on UK construction sites must meet BS EN 397 standards, which include tests for impact resistance, flame retardance, and other critical safety measures.
Shop Related Head Protection Categories